How to connect and "Receive" a new project file from an RC9 controller

Modified on Fri, Oct 11, 2024 at 8:10 PM

Please read our Legal Disclaimer before executing any steps on this article. 


Overview

Any time you need to send/receive changes to the RC9 robot program or parameters.


Tools and Parts Needed

PC with Wincaps III (latest version recommended - must be Windows 10 OS or higher) and an ethernet cable


Note:
If you are not sure which part number you need or the Robot Arm you own please stop and contact your DENSO Robotics sales representative.



Step by Step Guide


Step 1


Connect the ethernet cable to your PC and to the RC9 controller's LAN port (programming port)

Step 2


Open Wincaps III on your PC -> File -> New Project -> "Get information from the controller for creating a new project -> Next

Step 3


Select the name you want to call the project and the folder you want to save it in and click "Next"

Step 4


Enter the IP address of the robot (if it has been changed from the default) - Default IP address is 192.168.0.1 (PC must be on the same sub network  "192.168.0.XX" to communicate

Step 5


Select "Receive data from the controller" -> Finish

Step 6


The project will automatically save once transfer is complete. It is recommended to always keep a backup copy of the original project file that comes with your robot (also a backup copy of the project you are currently running).