NOTE:
Handle board with care.
Video Tutorial
Step-by-Step Guide
Pictures show a board that is currently setup for NPN.
Step 1Please jumper the two pins on JP6 and leave JP4 open. | ![]() |
Step 2Replace the 3 IC chips with the proper PNP type M54564P (410077-0020) 2021 UPDATE: 410077-0110 - NPN IC Chip 410077-0120 - PNP IC Chip | ![]() |
Step 3Short pins 2 and 3 on JP2 and JP5. | ![]() |
See in blue for additional information about RC7 I/O boards. “Switching procedure is the same for both”
There are two types of RC7 controller:
One controller has a safety box and the other a safety board. You can determine which I/O card is needed by the following:
If the I/O board has no chip it talks to the safety box. |
If the I/O board has a chip it talks to the safety board. Once this is determined see description and part number below for correct I/O board. |
If a new board is needed see reference below:
PNP type used with Safety Box - 410010-3290 |
NPN type used with Safety Box - 410010-3280 |
PNP type used with Safety Board - 410010-3270 |
NPN type used with Safety Board - 410010-3260 |
Was this article helpful?
That’s Great!
Thank you for your feedback
Sorry! We couldn't be helpful
Thank you for your feedback
Feedback sent
We appreciate your effort and will try to fix the article