Please read our Legal Disclaimer before executing any steps on this article.
Overview
Replace the encoder backup battery according to the procedure below. This procedure applies to the following robot types: VM-6083, VM-60B1
Tools and Parts needed
- Allen (hex) key
- Encoder backup battery for VM: - 410076-0080 - Encoder backup battery (SN 04E121 or earlier)
- 410611-0070 - Encoder backup battery (SN 04E122 or later)
 
Note:
If you are not sure which part number you need or the Robot Arm you own please stop and contact your DENSO Robotics sales representative.
Video Tutorial
Step by Step Guide
| Step 1Prepare a new set of 3 backup batteries for replacement. Note: |  | 
| Step 2Turn the controller power OFF. | |
| Step 3Remove the hexagon socket-head bolts (Allen bolts) from the battery support plate. |   | 
| Step 4Pull out the battery support plate from the robot unit. |  
 | 
| Step 5Remove the dummy connector cap from the battery board. |  | 
| Step 6Connect a new battery (1st one) to the pin from which you have disconnected the dummy connector cap in Step 5. NOTE: |  | 
| Step 7Disconnect the old backup battery that is left next to the new battery connected in Step 6, and then connect a new battery (2nd one). |  | 
| Step 8Disconnect the old backup battery that is left next to the new battery connected in Step 7, and then connect a new battery (3rd one). Note: |  | 
| Step 9Remove the last old battery and connect the dummy connector cap disconnected in Step 5. |  | 
| Step 10Secure the battery support plate to the connector plate. |   | 
Next Steps:
Owner's Manual Reference
https://www.fa-manuals.denso-wave.com/en/usermanuals/000895/