ORiN 2 - Programming in Visual C++ (CAO Engine)

Modified on Fri, 11 Jun 2021 at 04:25 PM

**Attention** : Read this resource material carefully and in its entirety before use, to ensure it is understood and used properly.  Failure to properly follow the instructions in the resource materials DPAM provides may result in damage to your equipment.  As a result, by using the resource materials, you are assuming the risks associated with modifying your equipment. DENSO holds no liability, implied or otherwise, for damage, injury or any legal responsibility incurred, directly or indirectly from the use of the resource materials, including any loss of data or damage to property which may occur by your use of the resource materials. The use of the resource materials are not recommended unless you have technical knowledge and functional experience with the equipment and related software. DENSO is unable to provide support, remote or otherwise, for the information included in the resource material, nor for the ancillary topics relating to the information included in the resource materials. Therefore, if you are not fully comfortable with it, we strongly recommend that you send your unit to one of our Regional Support Centers for repair.  The information contained in the resource materials are subject to change at the sole discretion of DPAM. 


Overview

In ORiN2 SDK, DCOM (Distributed Component Object Model) of Microsoft Corporation is adopted as a distributed object technology. The DCOM based CAO can be used from various program languages such as C++, JAVA, and Visual Basic.

This article is meant to help to gather information on resources that can help you get started with interfacing with the CAO Engine in C# (Visual Studio IDE). This article is not intended to aid you with programming in C/C++ nor how to use Visual Studio IDE. 


Tools and Parts needed


NOTE:
The following sample code is provided "AS IS" under the MIT License. Programming support service of C/C++ is out of warranty. Please note that we do not provide any programming support service beyond basic setup and troubleshooting. 


Previous Steps...

Please make sure that you have reviewed the ORiN2 - Overview article and that your RC controller is properly setup. You can use the CAOTester to make sure that your PC is ready to communicate with the controller. 


Set up your controller to accept messages from your PC.ORiN 2 - Robot Controller Setup (RC8 / RC8A / COBOTTA)
Test communication using CAO Tester applicationORiN 2 - Operation check using CAOTester (CAO Engine)
Add CAO_i.c Include Path to your Visual Studio project


Programming References

At this point, you should be ready to begin programming your application to interface with your robot controller. When connecting to the controller, you will need to specify the ORiN provider you are trying to use to establish communication. The provider differs based on the robot controller you are using. RC5, RC7, and RC7M controllers use the NetwoRC provider. RC8, RC8A, and COBOTTA controllers us the RC8 provider.

NetwoRC provider directory

C:\ORiN2\CAO\ProviderLib\DENSO\NetwoRC


RC8 provider directory

C:\ORiN2\CAO\ProviderLib\DENSO\RC8


NOTE:
Please consult the Owner's manual for information on how to program your DENSO Robot or details on specific robot commands. 


Programming using the Provider

The following samples are for performing various basic but essential operations. The samples are for connecting using the RC8 Provider.

For more information you can reference Section 4 RC8 Programming Using the Provider from the RC8 Provider User's Guide PDF document

 

RC8 Provider User Guide Samples in Visual C++

This document intends to give you a better experience when trying to implement a command in the provider. We have "translated" the original VB6 samples in Section 5.0 from the RC8 provider guide into Visual C/C++ language. Click here to download a copy.


More samples...

You can find Visual C++ samples in your install of the ORiN 2 SDK. Here are some recommendations:


RC8 Provider Samples

Sample NameDirectory Path
Joystick SampleC:\ORiN2\CAO\ProviderLib\DENSO\RC8\Samples\Joystick\VC2005
RobotC:\ORiN2\CAO\ProviderLib\DENSO\RC8\Samples\Robot\VC6
Robot (Simple)C:\ORiN2\CAO\ProviderLib\DENSO\RC8\Samples\Simple\Robot\VC6
Task (Simple)C:\ORiN2\CAO\ProviderLib\DENSO\RC8\Samples\Simple\Task\VC6
Variable (Simple)C:\ORiN2\CAO\ProviderLib\DENSO\RC8\Samples\Simple\Variable\VC6
TaskC:\ORiN2\CAO\ProviderLib\DENSO\RC8\Samples\Task\VC2005


NetwoRC Provider Samples

Sample NameDirectory Path
TaskC:\ORiN2\CAO\ProviderLib\DENSO\NetwoRC\Samples\Task\VC

Owner's Manual Reference