Please read our Legal Disclaimer before executing any steps on this article. 
Overview
Arm calibration, CALSET, must be performed when any of the motors is replaced or the encoder backup battery goes dead so that the position-related data retained in the encoder is lost.
The CALSET data is different on each robot.
CALSET data should be managed by the customer. Back up the CALSET data periodically, referring to "Backing up Projects".
Tools and Parts Needed
- Philips-head screwdriver (depends on model)
- Allen (hex) key (depends on model)
- CALSET Jig- 410192-0010 - 6th axis CALSET jig
 
Note:
If you are not sure which part number you need or the Robot Arm you own please stop and contact your DENSO Robotics sales representative.
Video Tutorial
Step by Step Guide
External Apperance
Step 1 - 1st Axis
Turning end in the positive direction (counterclockwise end when viewed from top)
Step 2 - 2nd Axis
Turning end in the negative direction
Step 3 - 3rd Axis
Turning end in the positive direction
Step 5 - 5th Axis
Turning end in the positive direction
Step 6 - 6th Axis
Turning end in the positive direction, which is set by a CALSET jig
Step 6.1 - Fit the stopper pin to of the CALSET jig for the right model

Step 6.2 - Install the CALSET jig on the 6th axis flange as shown in the figure below.

TIP: The CALSET position of the 6th axis refers to the point where the stopper pin (shown in the figure below) comes into contact with bolt (A) by turning the flange of the 6th axis.
Step 7 - Execute CALSET
NOTE: To perform this oepration, set the user level as "Maintainer"
Operation Path: [F2 Arm ] >> [F12 Maintenance] >> [F7 CALSET]
Step 7.1 - Press [F7 CALSET]
If you are swapping the arm or the controller you want to verify that the RANG data matches the robot. To review RANG data click [F3 Input Number]
Step 7.2 - Press [F1 CALSET]
Select some or all joints that require CALSET and then press the OK button to confirm selection.
| ROM ver. 2.7.* or Lower | ROM ver. 2.8.* or higher | 
Next Steps:
Owner's Manual Reference