Answer
There are a few different ways to find out if your RC8 or RC8A controller is currently configured for PNP or NPN I/O.
- The nameplate on the top of the controller lists the controller type. Character F signifies what the I/O type is at the time of manufacture.
- Another way to check is on the Teach Pendant:
- From the main screen -> Settings -> System Info -> General Tab

- Another way is to physically open the controller and view the Mini I/O card directly. The I/O type is screen printed on top of the card and can be viewed easily if there are no Fieldbus cards in the way