RC9
The RC9 controller with the VM-B and VL robots includes safety motion in addition to the standard safety inputs for emergency stops, protective stops, and e...
Tue, 22 Feb, 2022 at 1:43 PM
The RC9 IO cables EMC evaluation for noise is only tested up to 15m in length. However, these cables can be extended to 30m using the proper cable specif...
Tue, 22 Feb, 2022 at 1:47 PM
The RC9 with the VM-B and VL robots has safe motion as standard. Out of the box, it enables RLS and SS2. Thus, if you want to run the robot in AUTO, you mus...
Tue, 1 Mar, 2022 at 5:09 PM
The RC9 has multiple safety inputs that need to be wired in in order to operate the robot. Wiring is similar to RC8A in that you must wire in the emergen...
Tue, 22 Feb, 2022 at 1:53 PM
Overview This procedure needs to be done any time a new VL robot is being setup or you are pairing a different arm with an RC9 controller (replacing an arm...
Mon, 9 May, 2022 at 10:58 AM
Overview Any time you need to send/receive changes to the RC9 robot program or parameters. Tools and Parts Needed PC with Wincaps III (latest version ...
Fri, 6 May, 2022 at 12:55 PM
Overview Perform this procedure anytime the RC9 STO error 81501078 occurs Tools and Parts Needed RC9 robot controller and teach pendant. Note:
If...
Mon, 9 May, 2022 at 10:58 AM
Overview This procedure needs to be setup any time you want to connect a Denso RC9 controller to any Rockwell PLC using Ethernet IP Tools and Parts Nee...
Mon, 9 May, 2022 at 10:58 AM