Problem
Generated command value exceeded the speed limit. All joints were Emergency-stopped and motor power was turned OFF. On CP-motion or Pass-motion, the speed of each joint might change rapidly, so as to realize the target motion and pose of TCP.
Related Error codes:
84204061, 84204062, 84204063, 84204064, 84204065, 84204066, 84204067, 84204068
Solution
Double check your optimization settings after sending the project data. It is likely you may have reverted them to the default values.
This optimization can be setting via teach pendant or Wincaps III
Method #1: Setting the speed optimization from the teach pendant.
The controller must be in MANUAL mode to change the parameter. From the top screen on the teaching pendant, press the Arm button | |
Press the “Aux” button | |
Press the “Config” button | |
Confirm the correct settings are input for the Payload and CoG offsets are correct to your application | |
Scroll down to Config Parameter #8 and press “Edit” | |
Reference below for a description of each of the different modes. Once you have determined what setting you need, select it and press “OK” and then “OK” again. Optimal Speed Control Function |
Method #2: Setting the Speed optimization setting using Wincaps III
Open your current project file (Fresh upload is best) | |
Select “Project” from the top menu and then select “parameter…” Select your desired mode and click “OK” Download the parameters to your Controller |
Optimal Speed Control Function (Owner's Manual)
https://www.fa-manuals.denso-wave.com/en/usermanuals/001542/
Was this article helpful?
That’s Great!
Thank you for your feedback
Sorry! We couldn't be helpful
Thank you for your feedback
Feedback sent
We appreciate your effort and will try to fix the article