TABLE OF CONTENTS
- Extended-Joint Function
- Setup Example
- Step 1: Connect the Motor and Encoder (Robot side)
- Step 2: Connect encoder root cable
- Step 3: Connect extended axis encoder
- Step 4: Enable extended axis on the RC8
- Step 5: Connect power cable for extended axis.
- Step 7: Check encoder signal
- Step 8: Calibrate extended axis motor
- Step 9: Perform Auto Gain Tuning for extended Joint
- Step 10: Done (Jogging the extended axis)
- Other Resources
Extended-Joint Function
The extended-joint function allows you to control extra joints independently of robot joints through the standard interface of the robot controller (RC8 series).
The extended-joint support system is different from the conventional robot system in the following points.
- Robot controller which is equipped with a driver board suited to extended-joint motors to be connected.
- The robot controller and extended-joint motors are connected using extended-joint motor cables, motor conversion cables, encoder cables, and encoder backup batteries (all of these are options).
- Extended-joint motors (option) which are equipped with bus-line encoders. (6-axis robot: up to 2 motors. 4-axis robot: up to 4 motors. Motor type available)
Sample of components needed (controller on the image is an RC8)
Necessary Components
Encoder Hub
Part No. | Note |
410010-7100 |
Encoder Cable
Part No. | Length | Note |
410141-5950 | 1m | |
410141-5960 | 2m | |
410141-5970 | 3m | |
410141-5980 | 4m | |
410141-5990 | 6m | |
410141-6000 | 12m |
Motor Cable
Part No. | Length | Note |
410141-6020 | 2m | |
410141-9770 | 4m | |
410141-9780 | 6m | |
410870-9790 | 12m |
Encoder Backup battery
Part No. | Note |
410611-0030 |
Encoder Battery Cable
Part No. | Length | Note |
410141-6140 | 0.5m |
Servo Motor
Review the full list of AC Servo Motors https://www.fa-manuals.denso-wave.com/en/usermanuals/005479/
Power | Shaft Size | Options |
30W | 40mm | (brake)(oil seal) |
50W | 40mm | (brake)(oil seal) |
100W | 40mm and 60mm | (brake)(oil seal) |
200W | 60mm | (brake)(oil seal) |
400W | 60mm and 80mm | (brake)(oil seal) |
750W | 80mm and 100mm | (brake)(oil seal) |
1000W | 100mm | (brake)(oil seal) |
Driver Unit
Note: One driver powers 2 motors.
Part No. | Description |
410010-6120 | Driver Unit (L/S) |
410010-7150 | Driver Unit (L/SS) |
410010-6140 | Driver Unit (S/S) |
410010-7160 | Driver Unit (S/SS) |
410010-6550 | Driver Unit (SS/SS) |
Power rating of driver unit letter
Power Size | Motor |
SS | 30W, 50W, 100W |
S | 200W, 400W |
L | 750W, 1000W |
Example:
- To power a 750W and a 400W motors you need to use a L/S driver unit.
- To power a single 400W motor you need to use a S/SS driver unit.
- To power two 100W motors you need to use a SS/SS driver unit.
NOTE: It is not possible to power 2 750W or 2 1000W motors with a single driver unit since there is no L/L model.
Optional Components
Encoder Junction Cable
Part No. | Length | Note |
410141-5900 | 2m | |
410141-5920 | 4m | |
410141-5930 | 6m | |
410141-5940 | 12m |
Motor Junction Cable
Part No. | Length | |
410870-7130 | 1m | |
410870-7150 | 2m | |
410870-7170 | 3m | |
410870-7190 | 4m |
How many extra joints can I have?
How to mount the encoder hub?
Note: The encoder hub has the capability of being mounted on top of the RC8 controller as the image shows.
Setup Example
The following example assumes that your RC8/RC8A controller was originally purchased with the Extended Axis function.
Step 1: Connect the Motor and Encoder (Robot side)
Motor power from the robot will connect as usual (For a VS068 SLOT1, SLOT2, and SLOT3). | |
The encoder connector will go to the encoder hub port labeled as “Robot”. |
Step 2: Connect encoder root cable
Connect one end of the encoder into the controller and the other into the encoder hub.
Step 3: Connect extended axis encoder
Connect one end of the encoder junction cable to the extended joint motor. | |
Connect one end of the encoder junction cable to the encoder hub on the joint 7 slot. |
Step 4: Enable extended axis on the RC8
- Turn on the RC8 Controller
- Login as Maintainer and access Motor Settings.
Step 5: Connect power cable for extended axis.
Plug the connector on the correct slot and side. | |
Plug the connector on the motor side. |
Step 6: Connect Encoder Battery
Connect encoder battery. | |
Power ON RC8 |
Step 7: Check encoder signal
- Turn ON the RC8 controller
- Access Encoder Info page.
Step 8: Calibrate extended axis motor
- Login as Maintainer
- Access the CALSET page.
Step 9: Perform Auto Gain Tuning for extended Joint
- Check the separate article about how to perform auto tune test How to Auto Tune an RC8 Extended Axis/MC8 Controller
Step 10: Done (Jogging the extended axis)
To Jog the extended axis we need to click on the top button of the screen and select ExJoint before we try
moving the axis.
To Jog the extended axis we need to click on the top button of the screen and select ExJoint before we try moving the axis.
To Jog the extended axis we need to click on the top button of the screen and select ExJoint before we try moving the axis. |
Sub Main 'Get Arm Group 2 involving both robot 'joints and extended‐joints. TakeArm 2 Keep = 0 'Move robot flange to P0 as well as 'moving 7th and 8th extended‐joints to 'relative coordinates synchronously. Move P, P0 Ex ((7,30),(8,10)) 'Move robot flange to P1 as well as 'moving 7th extended‐joint to absolute 'coordinates synchronously. Move P, P1 ExA ((7,30)) End Sub
Other Resources
- Extended Joing Owner's Manual https://www.fa-manuals.denso-wave.com/en/usermanuals/004868/
Was this article helpful?
That’s Great!
Thank you for your feedback
Sorry! We couldn't be helpful
Thank you for your feedback
Feedback sent
We appreciate your effort and will try to fix the article