Error 8150202C “Specified field network device does not exist” for (RC8/RC8A)

Modified on Fri, Oct 11, 2024 at 6:34 PM

Please read our Legal Disclaimer before executing any steps on this article. 



Problem

If you see the following error this means that within your project the designated field bus is not set correctly.



Related Error codes:
8150202C 


Solution

To correct this error you will need to first open a fresh version of your Wincaps III project.


To correct this error you will need to first open a fresh version of your Wincaps III project.

Then you will go to Project -> Properties

Then select the I/O tab at the top and click on the drop-down arrow next to “Device”


Select the field bus card you have installed in your controller. If you do not have an additional card installed (DeviceNet, Ethernet IP, CC-Link, etc.) then you will need to select “Mini IO” and then click “OK”.


Then go to Connect -> Transfer Data -> Extend “Parameter” and check the I/O box -> Click “Send”

Once you have completed downloading your changes you will need to reboot your controller.

The error should be gone once the controller reboots



Owner's Manual Reference

https://www.fa-manuals.denso-wave.com/en/usermanuals/001061/