Exclusive Control Function for RC8/RC8A

Modified on Mon, Dec 30, 2024 at 11:11 AM

Please read our Legal Disclaimer before executing any steps on this article. 



Overview

 

DENSO robotics Exclusive Control function can prevent more than one robot from entering the exclusive area.

 

How does exclusive control work?

When more than one robot shares a work area, the exclusive control  function can limit entry into the work area to only one robot. The work  area used when the exclusive control function is used is called the  exclusive area. When robot "A" is about to enter the exclusive area that  another robot has already entered, the function prevents more than one  robot from entering the exclusive area by decelerating or stopping robot  "A."


 System Configuration 

Set up one robot controller as a mater controller  and others as  slave controllers. Up to four robots can be registered in one  exclusive  control group.  Connect the master controller  and slave controllers through a HUB.


DEMO Video


Owner's Manual