Panel Screens – Samples and Examples

Modified on Tue, 4 Mar, 2025 at 8:17 PM

Please read our Legal Disclaimer before executing any steps on this article. 


TABLE OF CONTENTS

Overview

Below are selections of panel screen samples and examples showing some options and combinations that can be made using the various functionalities available. 


Samples and Examples

Timer

Using a timer to view variables being sent from a camera.

Positions

Using a text box to view the current position of a robot (being read into a string variable via the PacScript program: S[4] = CurPos).

Displaying a Parsed String:

If the robot arm is palletizing or de-palletizing, the status of the pallet positions can be shown on the active panel screen.

Displaying System I/O

Displaying the System I/O can quickly show the status and activity of the controller.