VM-6083/VM-60B1 Series Robot Calibration (CALSET)

Modified on Tue, Nov 12, 2024 at 11:44 AM

Please read our Legal Disclaimer before executing any steps on this article. 


Overview

Arm calibration, CALSET, must be performed when any of the motors is replaced or the encoder backup battery goes dead so that the position-related data retained in the encoder is lost.

The CALSET data is different on each robot.

CALSET data should be managed by the customer. Back up the CALSET data periodically, referring to "Backing up Projects".


Tools and Parts Needed

  • Philips-head screwdriver 
  • Allen (hex) key
  • CALSET Jigs


Note:
If you are not sure which part number you need or the Robot Arm you own please stop and contact your DENSO Robotics sales representative.


Video Tutorial


Step by Step Guide (for all axis)

Previous Steps:


1st Axis

Step 1

Turning end in the positive direction (counterclockwise end when viewed from top) 



2nd Axis

Step 1

Turning end in the negative direction 



3rd Axis

Step 1

Turning end in the positive direction 



4th Axis (with mechanical stop)

Step 1

Models having no mechanical stop on the 4th axis Turning end in the positive direction, which is set by a CALSET jig. (counterclockwise end when viewed from the arm end) 

Step 2

Release the brake of the 4th axis. 


Step 3




4th Axis (without mechanical stop)

Step 1

Remove the 3rd-axis motor cover and unscrew the CALSET bolt.

NOTE: After CALSETing, be sure to set the bolt back into place and torque it to 1.0 Nm ±20%. 

Step 2

Rotate the second arm to the position specified in Step 4.

Step 3

Release the brake of the 4th axis.

Step 4

Set the CALSET bolt to the end of the 3rd axis housing as shown below.


Tightening torque of the CALSET bolt: 2.9 Nm ±20%


NOTE: Be sure to use the CALSET bolt as a CALSET jig. Using any other bolt will result in a positional error in CALSET. 


TIP: The CALSET position of the 4th axis refers to the point where the notch of the second arm comes into contact with the head of the CALSET bolt by turning the second arm. 



5th Axis

Step 1

Turning end in the positive direction (upward end of the 5th-axis arm) 


6th Axis

Step 1

Fit a stopper pin in the CALSET jig. 

Step 2

Release the brake of the 6th axis.  


Step 3

Install the CALSET jig on the flange of the 6th axis as shown in the figure below and the figure on the next page.


The CALSET position of the 6th axis refers to the point where the stopper pin (shown below) comes into contact with bolt (A) when the flange of the 6th axis is turned.




Next Steps:

Owner's Manual Reference

    

Was this article helpful?

That’s Great!

Thank you for your feedback

Sorry! We couldn't be helpful

Thank you for your feedback

Let us know how can we improve this article!

Select at least one of the reasons
CAPTCHA verification is required.

Feedback sent

We appreciate your effort and will try to fix the article