What happens to the arm odometer after an arm swap out with an RC7M?

Modified on Tue, Oct 22, 2024 at 6:40 PM

Please read our Legal Disclaimer before executing any steps on this article. 


The arm odometer doesn't reset automatically after you swap a new arm into an existing controller.  If the previous odometer data is needed, then the project backup will need to be loaded into the controller.


To access the RC7M odometer: 

            Set >> Maint >> Total h.



Step 1

On the top screen of the teach pendant, press [F6 Set].
The Settings (Main) window appears.


Step 2

Press [F6 Maint.] in the Settings (Main) window.
The Maintenance menu appears.


Step 3

Press [F1 Total h.] in the Maintenance menu.


 



Related Links: