Cobotta PRO, What's inside the box?

Modified on Mon, Jan 13, 2025 at 1:27 PM

Cobotta Pro – What is inside the box?

 

COBOTTA Collaborative Robots | DENSO Robotics

 

The Cobotta Pro is DENSO’s collaborative robot offering ranges of 900 mm and 1300 mm ranges along with respective payload capacities of 6 kg and 13 kg. This document describes what to expect when you order a Cobotta Pro robot with CRC9 controller.

 

Here is the Cobotta Pro in its original packaging from the factory.

Here is the robot package with the top box cover removed.

Robot shipping list attached to arm

Upon removing the plastic cover on the robot arm, you will notice a metal plate attached to the flange. This is a stabilizer for transporting the robot.

https://www.fa-manuals.denso-wave.com/en/COBOTTA%20PRO/016573/

 

Inside the controller box

Actual components descriptions inside the controller box can be found under the following link.

https://www.fa-manuals.denso-wave.com/en/COBOTTA%20PRO/016567/

Here is an image of the CRC9 controller