Can the Teach Pendant Buzzer be turned off?

Modified on Thu, Mar 20, 2025 at 1:51 PM

Can the beeping sound that is heard when using the TP-RC7/8 Full Size Teach Pendant be disabled or turned off?

Answer


No, the teach pendant buzzer cannot be disabled.  


If in a quiet environment, there are some options to help mitigate the sound of the buzzer: 


When using the teaching pendant.
- Using the Jump button instead of scrolling down: Displaying and Changing Variable Screen
- Pressing the SHIFT button and Down Arrow on the pendant is like a page down. 

Using Wincaps in Debug Mode
- Using Debugging (user manual link) Using Debugging
- Useful when testing a program (you can turn on the motor from Wincaps and see the program running from the PC 

Using Virtual TP application software from Robot Tools
- This allows you to view and navigate the teach pendant menu remotely from your PC (only in Manual Mode). 

Note: There will still be some things that you need the Teach Pendant for, like Jogging the robot.