Response
Physical robot speed is the same. However, due to constant I/O data transfer for every function block used the overall cycle time of a program would be slightly less than running a program internally from the controller.
Modified on: Wed, 28 Apr, 2021 at 2:19 PM
Physical robot speed is the same. However, due to constant I/O data transfer for every function block used the overall cycle time of a program would be slightly less than running a program internally from the controller.
Did you find it helpful? Yes No
Send feedback