**Attention**: Read this resource material carefully and in its entirety before use, to ensure it is understood and used properly. Failure to properly follow the instructions in the resource materials DPAM provides may result in damage to your equipment. As a result, by using the resource materials, you are assuming the risks associated with modifying your equipment. DENSO holds no liability, implied or otherwise, for damage, injury or any legal responsibility incurred, directly or indirectly from the use of the resource materials, including any loss of data or damage to property which may occur by your use of the resource materials. The use of the resource materials are not recommended unless you have technical knowledge and functional experience with the equipment and related software. DENSO is unable to provide support, remote or otherwise, for the information included in the resource material, nor for the ancillary topics relating to the information included in the resource materials. Therefore, if you are not fully comfortable with it, we strongly recommend that you send your unit to one of our Regional Support Centers for repair. The information contained in the resource materials are subject to change at the sole discretion of DPAM.
Problem
If your robot is not responding, and you are seeing these errors than one of your dual E-stop circuits was opened incorrectly. For the robot to function both E-stop circuits must be opened at the same time and from separate circuits.
This means you can’t have both circuits running through the same contact, they must be separate contacts if being used.
Related Error codes:
83400042, 85491006
Solution
NOTE: You should always power down the controller before changing/modifying your controller’s wiring configuration
The 2 E-stop circuits are shown above as the 2 twisted pairs of wires of RED/PINK and BROWN/PINK. This means when Pin #2 (brown) and Pin #36 (Pink) are shorted the controller sees E-stop signal. When Pin #3 (Red) and Pin #37 (Pink) are shorted the controller sees E-stop signal 2
You can see from the wiring diagram above how the E-stop safety signals should be wired. The contacts within the same rectangle are dual circuits and must be closed at the same time. Generally, these are 2 contacts on two different relays that have the coils triggered at the exact same time. This is for safety reasons in case 1 of the relays fails you have another to secure the safety circuit.
Check the wiring circuits for the referenced wires above and confirm they are wired correctly. The errors above tells you which circuit closed prematurely (circuit 1 or circuit 2)
You will need to correct any issues found and then open both circuits. You should then be able to reset the faults. You can then trigger your E-stop conditions to close both circuits at the same time and you should have no errors.
NOTE: It is the same condition requirements for the protective stop and auto enable circuit
Owner's Manual Reference
https://www.fa-manuals.denso-wave.com/en/usermanuals/002621/