Encoder System Down Failure

Modified on Fri, Oct 11, 2024 at 6:22 PM

Please read our Legal Disclaimer before executing any steps on this article. 


Overview

Applicable Errors: 

85404671 - J1 encoder system down  

85404672 - J2 encoder system down 

85404673 - J3 encoder system down 

85404674 - J4 encoder system down 

85404675 - J5 encoder system down 

85404676 - J6 encoder system down 

85404677 - J7 encoder system down 

85404678 - J8 encoder system down 

 

Error Description: 

Failed to read the encoder information of the corresponding axis. 

 

Possible Causes: 

1.Dead Batteries in the robot. Batteries inside of the robot operate at 3.6V +/- 20%. If the batteries are low the batteries in the robot arm need to be replaced, the affected encoder(s) need to be reset, cycle power on the controller,   

 

2. A motor was changed or was unplugged from the wiring harness inside of the robot arm. To resolve this error - confirm affected joints, reset encoder(s), cycle power on the controller, and calibrate robot.  

 

3.Temporary disconnection of the power conversion board inside of the robot.  

 

4. A motors encoder has become damaged. Exchange the motor, reset encoder, calibrate affected joint. 

 

 

Remedy: 

Identify and resolve the cause of the error and then reset the encoder using the guide below


Tools and Parts Needed

Full Sized Teaching Pendant  



Step by Step Guide


Step 1 

Confirm affected joint(s) by using the full sized teaching pendant 


Displaying Encoder Information (denso-wave.com) 

Step 2 

Identify the affected joint(s) 

Joint(s) affected by this error can be identified by a red circle in the System Status column.  
 

Step 3 

Reset encoder(s) for affected joint(s) 


 Resetting Encoder (RC8 / RC8A) : DENSO Robotics KB (freshdesk.com) 

Step 4 

Cycle power on your controller. 



Step 5 

Calibrate all joints that were reset.


How do I perform a CALSET for the robot? : DENSO Robotics KB 


Next Steps:

  • For repair options in the Americas please contact support@densorobotics.com 

  • For repair options outside of the Americas, please contact your local Denso Service Center.