Please read our Legal Disclaimer before executing any steps on this article.
Overview
Applicable Errors:
84404571 – J1: Motor Overcurrent
84404572 – J2: Motor Overcurrent
84404573 – J3: Motor Overcurrent
84404574 – J4: Motor Overcurrent
84404575 – J5: Motor Overcurrent
84404576 – J6: Motor Overcurrent
84404577 – J7: Motor Overcurrent
84404578 – J8: Motor Overcurrent
844044B1 – J1: Excessive current error
844044B2 – J2: Excessive current error
844044B3 – J3: Excessive current error
844044B4 – J4: Excessive current error
844044B5 – J5: Excessive current error
844044B6 – J6: Excessive current error
844044B7 – J7: Excessive current error
844044B8 – J8: Excessive current error
84404431 – J1: Driver unit Overcurrent (U-Phase)
84404432 – J2: Driver unit Overcurrent (U-Phase)
84404433 – J3: Driver unit Overcurrent (U-Phase)
84404434 – J4: Driver unit Overcurrent (U-Phase)
84404435 – J5: Driver unit Overcurrent (U-Phase)
84404436 – J6: Driver unit Overcurrent (U-Phase)
84404437 – J7: Driver unit Overcurrent (U-Phase)
84404438 – J8: Driver unit Overcurrent (U-Phase)
84404441 - J1: Driver unit Overcurrent (V-Phase)
84404442 – J2: Driver unit Overcurrent (V-Phase)
84404443 – J3: Driver unit Overcurrent (V-Phase)
84404444 – J4: Driver unit Overcurrent (V-Phase)
84404445 – J5: Driver unit Overcurrent (V-Phase)
84404446 – J6: Driver unit Overcurrent (V-Phase)
84404447 – J7: Driver unit Overcurrent (V-Phase)
84404448 – J8: Driver unit Overcurrent (V-Phase)
Error Description:
Current flow through the motor or the driver unit of the corresponding axis exceeded the permitted value.
Possible Remedy:
- Reduce the robot speed, acceleration and deceleration.
- Confirm the end of arm load is not in excess of parameter value & arm capacity.
- Motor encoder cable broken.
- Robot is not colliding with any external obstacle.
- Driver Unit failure
- Robot internal wiring is damaged.
- Mechanical failure of drive component in specified joint
- Motor failure
Tools and Parts Needed
Full Sized Teaching Pendant
#2 Phillips Screwdriver
Hex Wrench Set
Step by Step Guide
Step 1Confirm the end of arm load is not in excess of parameter value & arm capacity. |
|
Step 2Verify the motor encoder cable is not broken or damaged. |
|
Step 3Robot is not colliding with any external obstacle. |
|
Step 4Verify Driver unit operation. |
|
Step 5Verify no damage to wiring harness inside of robot. |
|
Step 6 Verify there is no mechanical failure of drive component in specified joint. |
|
Step 7Motor failure |
|
Next Steps:
- For repair options in the Americas please contact [email protected]
- For repair options outside of the Americas, please contact your local Denso Service Center.
Owner's Manual Reference
Was this article helpful?
That’s Great!
Thank you for your feedback
Sorry! We couldn't be helpful
Thank you for your feedback
Feedback sent
We appreciate your effort and will try to fix the article