Please read our Legal Disclaimer before executing any steps on this article.
Overview
Starting and stopping your Supervisory Tasks (TSR#) can be done through the PLC I/O (Standard Allocation Mode Only). It is very similar to calling a normal program but with slightly different data.
The robot has 3 system data areas that it looks at for commands whenever the strobe signal is pulsed “High”
  | ![]() ![]()  | 
Start a single Supervisory Task
To start a single Supervisory Task you would move the following data in the data areas as shown in the manuals
Command Data Area = 0001 or “1”
Data Area 1 = 10000000 or “128”
Data Area 2 = # of tsr program in Binary (tsr5 = 00000101 or “5”)
Once data is input then pulse the “Strobe” Signal and the supervisory task will start
Stop a single Supervisory Task
To stop a single Supervisory Task you would move the following data in the data areas as shown
Command Data Area = 0001 or “1”
Data Area 1 = 10000001 or “129”
Data Area 2 = # of tsr program in Binary (tsr5 = 00000101 or “5”)
Once data is input then pulse the “Strobe” Signal and the supervisory task will start
Start all Supervisory Tasks
To start running all Supervisory Tasks (TSR) in the controller then you would use the following sequence
Command Data Area = 0001 or “1”
Data Area 1 = 10000000 or “128”
Data Area 2 = 1111 1111 1111 1110 or “65,534(dec.) or FFFE(hex)”
Once data is input then pulse the “Strobe” Signal and the supervisory tasks will start
Stop all Supervisory Tasks
To stop running all Supervisory Tasks (TSR) in the controller then you would use the following sequence
Command Data Area = 0001 or “1”
Data Area 1 = 10000000 or “128”
Data Area 2 = 1111 1111 1111 1111 or “65,535(dec.) or FFFF(hex)”
Once data is input then pulse the “Strobe” Signal and the supervisory tasks will stop
Owner's Manual Reference
https://www.fa-manuals.denso-wave.com/en/usermanuals/000492/