FAQ
Response You can find a summary of the changes from RC7M to the RC8 controller listed at the link below. This summary includes both hardware and software ...
Tue, 8 Jun, 2021 at 9:48 AM
Response No, you should never unplug or plug in the pendant while the controller power is on. Always power down the controller and wait a few seconds bef...
Wed, 7 Jul, 2021 at 3:46 PM
Response The Short Circuit Current Rating (SCCR) is as follows for the controllers listed below. This information should also be listed on the controller ...
Tue, 27 Apr, 2021 at 7:27 PM
Response Only the IO that is relative to the e-stop or motor running will stop. All user outputs with still be in their state at the time of interruption a...
Tue, 25 May, 2021 at 1:13 PM
Obtaining a UL/CE Certificate for Robot Controller (RC8/RC8A) In order to obtain a UL or a CE certificate for your purchased DENSO robot controller, ple...
Wed, 7 Jul, 2021 at 1:18 PM
Summary Is it possible to sync the RC8/RC8A controller clock using an NTP server? Answer There is no feature to sync the clock of the RC8 controller v...
Fri, 11 Jun, 2021 at 5:48 PM
Response Yes, you must have a teach pendant plugged in for UL/CSA certification requirements
Tue, 8 Jun, 2021 at 9:49 AM
Response Yes, the RC7 teach pendant will work on the new RC8, and RC8A robot controllers with mostly similar functionality and navigation locations.
Wed, 26 May, 2021 at 12:34 PM
Response If a level 5 error has been generated on your DENSO Robot then you must reboot the controller to clear the error. If the cause of the error has no...
Tue, 8 Jun, 2021 at 9:48 AM
**Attention**: Read this resource material carefully and in its entirety before use, to ensure it is understood and used properly. Failure to properly foll...
Wed, 28 Apr, 2021 at 2:01 PM