Overview
Applicable Errors:
6411 - J1 encoder system down failure
6412 - J2 encoder system down failure
6413 - J3 encoder system down failure
6414 - J4 encoder system down failure
6415 - J5 encoder system down failure
6416 - J6 encoder system down failure
6417 - J7 encoder system down failure
6418 - J8 encoder system down failure
Error Description:
Failed to read the encoder information of the corresponding axis.
Possible Causes:
1.Dead Batteries in the robot. Batteries inside of the robot operate at 3.6V +/- 20%. If the batteries are low the batteries in the robot arm need to be replaced, the affected encoder(s) need to be reset, cycle power on the controller,
2. A motor was changed or was unplugged from the wiring harness inside of the robot arm. To resolve this error - confirm affected joints, reset encoder(s), cycle power on the controller, and calibrate robot.
3.Temporary disconnection of the power conversion board inside of the robot.
4. A motors encoder has become damaged. Exchange the motor, reset encoder, calibrate affected joint.
Remedy:
Identify and resolve the cause of the error and then reset the encoder using the guide below.
Tools and Parts Needed
Full Sized Teaching Pendant
Step by Step Guide
Step 1 Confirm affected joint(s) by using the full-sized teaching pendant. | From the main screen of the pendant select – Arm –Shift – Maint – ENC INF. |
Step 2 Identify the affected joint(s) | Joint(s) affected by this error can be identified by a black square in the System Status column. |
Step 3 Reset encoder(s) for affected joint(s) | Resetting Encoder (RC7 / RC7M) : DENSO Robotics KB |
Step 4 Cycle power on your controller. | |
Step 5 Calibrate all joints that were reset. | How do I perform a CALSET for the robot? : DENSO Robotics KB |
Next Steps:
For repair options in the Americas please contact support@densorobotics.com
For repair options outside of the Americas, please contact your local Denso Service Center.
Was this article helpful?
That’s Great!
Thank you for your feedback
Sorry! We couldn't be helpful
Thank you for your feedback
Feedback sent
We appreciate your effort and will try to fix the article