DENSO Robotics Controller Protective Enclosures

Modified on Fri, Nov 6 at 12:28 PM


Introduction

The DENSO Robotics Controller Protection box and Controller Protection Box Light are protective enclosures designed specifically for the DENSO RC8 and RC8A series controllers. The protective enclosures help to prevent costly contamination related failures and machine down time. It is generally recommended to implement the controller protection box at the time of machine integration, however many users have installed them after it became apparent that heavy contamination has resulted in controller damage. 

 




The two variations of the controller protection box exist to account for cooling capacity and cost. 


The standard Controller Protection Box has cooling capacity to address all configurations of the RC8 and RC8A series robot controllers except for UL specification it is at a higher cost than the Controller Protection Box Light. 


The Controller Protection Box Light while less expensive than the standard Controller Protection Box is compatible with all models except for UL specification controllers, controllers designed to operate the VM series robot, VSA4 series robots with additional axis control, and MC8 systems with a combined motor capacity of 2000W or higher.


Key Features


Controller Protection Box specifications:

ItemSpecifications
Applicable controllerRC8 series robot controller except UL models
Environmental conditions (Temperature and humidity)In operation0 to 40 ℃, 20 to 90% RH (dew condensation not allowed)
In storage or during transportation-10 to 60 ℃, 40 to 75% RH (dew condensation not allowed)
EnclosureEquivalent to IP54
Installation TypeStand-alone Installation (cannot be installed vertically)
Weight (Mass)Approx. 26 kg (RC8 series robot controller is not included)
Power supply
Note: the power supply of the controller protection box is not always the same as the controller
Three-phaseAC185-253 V(AC200 V-7 %~AC230 V+10 %)
Single-phaseAC207-253 V(AC230 V±10 %)
Heat exchangerFansInternal fan and external fan
External fan: 4715HS-23W-B50-AM0 (Manufactured by Minebea Co.,Ltd)
Internal fan : 4715MS-23W-B50-A00 (Manufactured by Minebea Co.,Ltd)
Cooling power35 W/K (temperature change 1 ℃ , calculated value)
Power supplySupplied from the controller power and branched by the protective box-incorporated terminal.
Power supply capacity: 0.15KVA



Controller Protection Box Light specifications:

ItemSpecifications
Applicable controllerRC8 series robot controller except UL series controllers, VM models, VSA4 with additional axis models, and MC8 systems with combined motor capacity in excess of 2000W
Environmental conditions (Temperature and humidity)In operation0 to 40 ℃, RH 90 % or below
(dew condensation not allowed)
In storage or during transportation-10 to 60 ℃, RH 75 % or below
(dew condensation not allowed)
EnclosureEquivalent to IP54
Installation TypeStand-alone installation, upright installation. Note: Upright instillation does require additional bracketry sold separately.
Weight (Mass)Approx. 18 kg (RC8 series robot controller is not included)
Power supply
Note: the power supply of the controller protection box is not always the same as the controller
Three-phaseAC185-253V (AC200V-7%~AC230V+10%)
Single-phaseAC207-253V (AC230V±10%)
Heat exchangerFansInternal fan and external fan
External fan: 11938SB-B3N-LAU-0 (Manufactured by Minebea Co.,Ltd)
Internal fan : 11938SB-B3N-JP-00 (Manufactured by Minebea Co.,Ltd)
Cooling power25 W/K (temperature change 1 ℃ , calculated value)
Power supplySupplied from the controller power and branched by the protective box Light-incorporated terminal.
Power supply capacity: 0.15 KVA




Connectivity & Integration

The Controller Protection Box and Controller Protection Box Light allow controllers to interface to all typical external devices normally by passing all cabling through a rubber wire clamps which helps prevent contamination ingress into the protection box.  

Due to the size of the protection box, it is recommended to use the box at time of machine integration.  Installing the protective box into an existing machine is possible however there may be difficulties depending on available space inside of the machine. It is recommended to review the full protective box documentation to ensure proper clearance is available inside the machine prior to purchasing the Controller Protection Box. 




Use Cases & Applications

Common applications:

  • Applications where the controller is exposed to excessive solid contamination, or fluid contamination such as machine tending.

Benefits

Benefits include:

  • Reduction of controller failures due to contamination which can interrupt production
  • Reduction of costly contamination related failures. 
  • Reduction of heat related errors

Resources & Documentation

Resources:

  • RC8(A) User Manual - See Controller & IO section - Controller Protective Box Manual / Controller Protective Box Light Manual.  

Support & Contact


For assistance, contact support@densorobotics.com or visit our online contact form at https://www.densorobotics.com/contact/

Was this article helpful?

That’s Great!

Thank you for your feedback

Sorry! We couldn't be helpful

Thank you for your feedback

Let us know how can we improve this article!

Select at least one of the reasons
CAPTCHA verification is required.

Feedback sent

We appreciate your effort and will try to fix the article