Please read our Legal Disclaimer before executing any steps on this article.
Overview
Here is a solution for sending local or global variables from the controller to the PLC by using the DEFIO command to assign values to Fieldbus IO sets.
Answer
One way to send a global or local variable from your robot program to your PLC is by defining a variable string to use by using the DefIO command. Review the command specifically here:
What our example will show here is sending from the robot to the PLC.

- DefIO Int2IO = byte, 820
- This line is using the DEFIO command to define our custom IO named "Int2IO". It is sized at 1 byte (8-bits), and starts at IO number 820.
- I[2] = 22
- This is simply giving the Global Integer variable, I[2], a value of 22
- Int2IO = I[2]
- This line is setting our custom IO, Int2IO, equal to the Global Variable I[2], thus equal to 22.
- After this happens, you can see that the bits/IO's in our custom IO take on the bit pattern to equal 22, but in Binary
- The trick to seeing this is to realize that the most significant bit is the highest IO, and the least significant bit is the lowest IO. In this case the MSB is 827, and the LSB is 820. So if you read it from the bottom up in the picture, it's 0001 0110, thus equalling 22 in binary.