DENSO's RC8/A controller allows the use of analog signals. This guide details what is required and how to set up this function.
Required Items:
RC8 Controller w/ Contec Motion Control Board
Provider enabled

RC8 mini IO connector (safety I/O connections)
RC8 power cable
Optional: RC8 teaching pendant
Contec AIO‐121601M‐PCI card 12‐bit analog card

EPD‐96 screw terminal

PCB96PS‐1.5P cable

Instructions
1. Input AIO board license key into RC8 extensions menu.
This license is free and can be generated from Denso Wave’s website.
https://www.denso-wave.com/en/robot/
2. Refer to Denso RC8 Owners Manual set for how to input provider license keys
Installing the AIO Card
1. Remove RC8 top cover
2. Remove screws mounting the PCI slot holder. The screws in the front are circled in black on the controller.


3. Remove holder and install AIO board. Secure board to holder with the screw that was used for the dust cover.


4. Reinstall holder and board into RC8 controller
Wiring
1. Connect PCB96P5‐1.5P cable between the AIO board and EPD‐96 screw terminal unit


2. Short all unwanted analog inputs to ground. Failing to do so will cause all the inputs to read from the other analog ports
3. Wire in your analog sensor to desired analog input port.
4. For this case, we used analog input AI0. Please see EPD‐96 pinout.

5. We also wired a volt meter to the analog output to test the analog output voltage.
Sample Panel

Panel Code
#include <PanelMain.h> raw
Dim g_ctrl as Object 'For CaoController object
Dim g_varAO0 As Object 'For variable object used to access the AIO board
Dim g_varAI0 as Object 'For variable input
Dim g_varAI1 as Object 'For variable input
Dim g_varAI2 as Object 'For variable input
Dim g_varAI3 as Object 'For variable input
Dim g_varAI4 as Object 'For variable input
Dim g_varAI5 as Object 'For variable input
Dim g_varAI6 as Object 'For variable input
Dim g_varAI7 as Object 'For variable input
Dim g_varAI8 as Object 'For variable input
Dim g_varAI9 as Object 'For variable input
Dim g_varAI10 as Object 'For variable input
Dim g_varAI11 as Object 'For variable input
Dim g_varAI12 as Object 'For variable input
Dim g_varAI13 as Object 'For variable input
Dim g_varAI14 as Object 'For variable input
Dim g_varAI15 as Object 'For variable input
Sub Panel_INITIALIZE()
On Error Goto ErrorProc
'Establish (open) connection
g_ctrl = cao.AddController("AIO", "CaoProv.CONTEC.AIO","","DeviceName=AIO000")
'Acquire device name
DeviceName.Caption = g_ctrl.AddVariable("@DeviceName").Value
'Create variable object(Specify data size(8bit))
g_varAO0 = g_ctrl.AddVariable("AO0")
g_varAI0 = g_ctrl.AddVariable("AI0", "")
g_varAI1 = g_ctrl.AddVariable("AI1")
g_varAI2 = g_ctrl.AddVariable("AI2")
g_varAI3 = g_ctrl.AddVariable("AI3")
g_varAI4 = g_ctrl.AddVariable("AI4")
g_varAI5 = g_ctrl.AddVariable("AI5")
g_varAI6 = g_ctrl.AddVariable("AI6")
g_varAI7 = g_ctrl.AddVariable("AI7")
g_varAI8 = g_ctrl.AddVariable("AI8")
g_varAI9 = g_ctrl.AddVariable("AI9")
g_varAI10 = g_ctrl.AddVariable("AI10")
g_varAI11 = g_ctrl.AddVariable("AI11")
g_varAI12 = g_ctrl.AddVariable("AI12")
g_varAI13 = g_ctrl.AddVariable("AI13")
g_varAI14 = g_ctrl.AddVariable("AI14")
g_varAI15 = g_ctrl.AddVariable("AI15")
Exit Sub
ErrorProc:
End Sub
Sub Panel_TERMINATE()
cao.Controllers.Remove g_ctrl.Index
g_ctrl = Nothing
End Sub
Sub Output_CLICKED()
'Output specified voltage value
g_varAO0.value = DC.Value
F0 = DC.value
End Sub
Sub Timer1_TIMER()
NB1.value = g_varA0.value
F2 = g_varAI0.value
NB2.value = g_varAI1.value
F3 = g_varAI1.value
NB3.value = g_varAI2.value
F4 = g_varAI2.value
NB4.value = g_varAI3.value
F5 = g_varAI3.value
NB5.value = g_varAI4.value
F6 = g_varAI4.value
NB6.value = g_varAI5.value
F7 = g_varAI5.value
NB7.value = g_varAI6.value
F8 = g_varAI6.value
NB8.value = g_varAI7.value
F9 = g_varAI7.value
NB9.value = g_varAI8.value
F10 = g_varAI8.value
NB10.value = g_varAI9.value
F10 = g_varAI9.value
NB11.value = g_varAI10.value
F11 = g_varAI10.value
NB12.value = g_varAI11.value
F12 = g_varAI11.value
NB13.value = g_varAI12.value
F13 = g_varAI12.value
NB14.value = g_varAI13.value
F14 = g_varAI13.value
NB15.value = g_varAI14.value
F15 = g_varAI14.value
NB16.value = g_varAI15.value
F16 = g_varAI15.value
End Sub
Sub FK1_CLICKED()
page_change main
End Sub
Additional Notes
• 16 analog input channels
• 1 analog output
• Input voltage range +/‐ 10V
• Output voltage range +/‐ 10V