Motor & Encoder Angled connector direction

Modified on Tue, 22 Feb 2022 at 01:34 PM

The 90 degree motor/encoder connector cannot be modified. If a customer requires this connector to point at a different angle, they would need to disconnect the motor/encoder male connect at the base of the robot arm and rotate it in 90 degree increments to the desired angle. You must be careful not to over rotate this connection as it can damage the robot’s internal wiring harness.