I/O Device Changed

Modified on Wed, Oct 16, 2024 at 5:02 PM

Please read our Legal Disclaimer before executing any steps on this article. 


Overview

Applicable Errors: 

 

220F 

 

 

Error Description: The status or configuration of I/O devices has been changed since 

the last time the controller was powered on. 

 

 

 

Possible Causes: 

 

1. An I/O expansion card has been installed or removed from the inside of the controller and the software configuration and hardware settings are no longer compatible. 

 

2. The I/O card in the controller has failed and is no longer detected by the controller. (replace card if damaged).  

 

3. A new project has been sent to the controller. The I/O settings in the project do not match the hardware installed inside of the controller.  

 

 

Remedy: 

 

  • Ensure the hardware in the controller aligns with the software installed in the controller.   



Tools and Parts Needed

Full Sized Teaching Pendant  



Step by Step Guide

Step 1 

Identify what your I/O configuration should be to communicate with your machine. (EX - Standard mode / Compatible mode / Mini IO assign, etc.) 


Step 2 

Using the full sized teaching pendant navigate to – IO -> Aux -> AlocMode. 



 

Step 3 

Select the configuration your machine was integrated with (Mini IO assign / Compatible / Standard, etc.). Select OK. 



Step 4 

Cycle power on your controller. Upon bootup the error should no longer be generated. Confirm robot controller / PLC handshaking works correctly. 



Step 5 

 If you continue to experience the 220F error, you may need to investigate having the controller repaired.  



Next Steps:

Use the RC7 Options Manual to confirm the I/O mapping of your machine & make note of IO setting on controller cover for future use.  

  • For repair options in the Americas please contact support@densorobotics.com 

  • For repair options outside of the Americas, please contact your local Denso Service Center. 


Owner's Manual Reference

Download RC7 Manual Pack to aid in determine the correct controller configuration- CADs and Manuals - DENSO Robotics 

Was this article helpful?

That’s Great!

Thank you for your feedback

Sorry! We couldn't be helpful

Thank you for your feedback

Let us know how can we improve this article!

Select at least one of the reasons
CAPTCHA verification is required.

Feedback sent

We appreciate your effort and will try to fix the article