Overview
Follow these steps if you run into a 60C4, path file creation error on RC7M.
Tools and Parts Needed
List if there are any tools or parts needed.
Note: If you are not sure which part number you need or the Robot Arm you own please stop and contact your DENSO Robotics sales representative.
Step by Step Guide
Step 1 | Inside Wincaps3, go to PROJECT > ADD PROGRAM > create a random program (let's call it TEST) |
Step 2 | After creating the program, click PROJECT > MAKE EXECUTABLE > if it compiles good go ahead and save your PROJECT |
Step 3 | After saving, click CONNECT > TRANSFER DATA > Select everything under Programs > click send |
Step 4 | After send is complete, reboot the controller > under Wincaps again > CONNECT > TRANSFER DATA > select all parameters > click SEND > Reboot |
Was this article helpful?
That’s Great!
Thank you for your feedback
Sorry! We couldn't be helpful
Thank you for your feedback
Feedback sent
We appreciate your effort and will try to fix the article