Please read our Legal Disclaimer before executing any steps on this article
Overview
A work offset is defined by moving the origin of the robots coordinate system to an offset distance from its default location. The default location is known as Work 0 and cannot be changed. Subsequent work offsets are labeled as Work 1, Work 2 and so on.
When developing an application, it can be very useful to have a work coordinate plane that is at an angle; to either match the contours of an existing work piece, or match the fixtures the robot arm is working with.
In the DENSO programming environment, there are 3 ways this can be done: Manual Entry, Easy Edit, and programmatically.

Method #1: Manual Entry

Method #2: 3-Point Teaching Method

Method #3: Program Entry
You can enter and define your work coordinate systems directly inside your programs if you desire. See the commands below:
'!TITLE "Robot program"
Sub Main
TakeArm Keep = 0
Work 1, P(0,0,0,0,0,45)
'Defines Work1 as a 5 degree Rotation in the Z plane
Work 2, P(100,100,50,0,0,0)
'Defines Work2 with a 100mm offset in the X and Y planes, and a positive 50mm in the Z.
ChangeWork 1
'Changes work to Work1
End Sub
3-point teaching PACScript function (custom)
If you would like to create a work offset based on 3 points similar to the teach pendant menu. You can use a sample function to create one on GitHub.
https://github.com/DENSO-2DLab/RC8_Function-EasyWork/releases/tag/v2.1.1
'!TITLE "Generate Work Offset"
#Include "EasyWork.pcs"
Sub Main
Dim Point1 As Position
Dim Point2 As Position
Dim Point3 As Position
Dim newWork As Position
Point1 = (-160, -200, 180, 0, 0, 0, -1) 'New Work Center
Point1 = (-300, -160, 240, 0, 0, 0, -1) 'New Work X Axis
Point1 = (-230, -270, 270, 0, 0, 0, -1) 'New Work XY Quadrant
newWork = EasyWork(Point1, Point2, Point3) 'Generate New Work Coordinate
Work 1, newWork
End SubDefining Work Offset in WinCAPS III
WINCAPS III also allows viewing and editing of Work coordinate systems in its environment:
| ![]() ![]() |
Owner's Manual Reference
https://www.fa-manuals.denso-wave.com/en/usermanuals/001743/