Legacy Equipment
Problem Although a serious error of Level 5 or higher one had occurred, you attempted to perform operation without recovery from error. Not able to move th...
Mon, 28 Feb, 2022 at 5:04 PM
Overview Programs, parameters, CAL data, etc. are stored in the internal memory of the robot controller. The memory backup battery retains the above da...
Tue, 27 Jul, 2021 at 5:50 PM
This article applies for the RC7 or RC5 Controller Problem When the controller powers up the 2AF1 error shows on the pendant. Typically this error ...
Wed, 21 Jul, 2021 at 12:58 PM
Overview External Auto Mode in the RC7 allows an external device (such as a PLC through System I/O) to start and stop programs, and issue other System I/O ...
Wed, 12 May, 2021 at 5:46 PM
NOTE: Handle board with care. Video Tutorial Step-by-Step Guide Pictures show a board that is currently setup for NPN. Step 1 Please jum...
Wed, 28 Jul, 2021 at 1:47 PM
Overview The following explains the encoder resetting procedure. Tools and Parts needed Full size Teach Pendant to follow this menus. 410...
Wed, 21 Jul, 2021 at 12:48 PM
Overview After replacing the memory backup battery, set the next battery replacement date from the teach pendant, according to the following procedure. No...
Fri, 25 Feb, 2022 at 7:31 PM
**Attention**: Read this resource material carefully and in its entirety before use, to ensure it is understood and used properly. Failure to properly foll...
Wed, 12 May, 2021 at 6:17 PM
Overview The RC7M controller uses fuses for its outputs to prevent damage due to overcurrenting. The fuses typically blow when a particular output is short...
Tue, 20 Jul, 2021 at 7:31 PM
**Attention**: Read this resource material carefully and in its entirety before use, to ensure it is understood and used properly. Failure to properly fo...
Wed, 12 May, 2021 at 6:39 PM